This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2373: Controller can be paired with TPS2373

Part Number: TPS2373
Other Parts Discussed in Thread: LM5155, UCC2897A, , , , TIDA-050045

Hello there:

Due to the component shortage problem of LM5155, I am wondering what are the alternative options to replace with LM5155 when use that as a PoE++ power supply design. Right now I think LM5155/5156/5157/5158 are possible options, and on the evaluation board TI uses UCC2897A as a controller. I am looking for more options, thank you so much in advance!

  • Hello Ryan, 

    I am on the Power Over Ethernet team, and the LM5155 and UCC2897's don't fall under our product line. I think to get the best response for new parts, please create a new post and tag only those parts. 

    In this power space, we have a new part, The TPS23730, which integrates the TPS2373 and the DCDC controller. It supports up to 51W. This could help eliminate a part in the BOM. 

    Please see the TPS23730EVM-093 for a 12V solution and TIDA-050045 for a 5V solution. 

    If this post answers your question, please indicate so by marking this thread as resolved. Thank you.

     

    Regards, 

     

    Michael P.

    Applications Engineer

    Texas Instruments