Other Parts Discussed in Thread: TPS628501
Hello,
In the datasheet of TPS628501-Q1 there is the following description regarding the output short circuit protection:

So as I understand, in a short circuit condition, the high-side MOSFET will switch off, and will be turned on again after the current drops below the current limit of the low-side MOSFET, which will always happen as when the HS MOSFET is turned on, there is no power supplied to the short circuit. => therefore the converter will never turn off its output during a short circuit on the output.
Below a measurement done during the application of a hard-short (less than 50mOhm) directly on the output of the TPS628501. The converter does not turn off. Is this the correct/expected behavior ?