Hi Team,
I have three questions about TPS6508641 so could you support?
device: TPS6508641
#1: LDOAx
What is the difference between 7.9 electrical characteristics: LDOA1/2/3 tstartup ~500us_max vs 7.15 Switching Characteristics
LDOAx tstartup 180us_typ?
#2: minimum start-up time
What is the minimum tpg(total turnon time) of BUCK CONTROLLERS, BUCK CONVERTERS, LDOAx, SWA1 and SWB1_2?
MPSoC requires 0.2ms_minimum ramp time from GND to 95% of Vcc_xxx.
#3: LDOAx minimum start-up time with 2.2, 4.6 or 10uF output capacitor
LDOAx startup time is "Measured from EN = H to reach 95% of final value".
this means LDOAx start-up time should be controled internally inspite of output voltage.
Even if we change output capacitor from 4.7uF to 2.2 or 10uF, we can apply the same LDOAx start-up time of #2 answer of LDOAx minimum startup time?
Regards,
Kai