This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS543620: Only switching a 2MHz

Part Number: TPS543620

Hello,

We have a well regulated supply. Nevertheless we are not able to change the switching frequency. It was designed for 1MHz (11.8Kohm resistor to ground on pin 1) but it always goes to 2MHz. We tried changing it to 26KOhms to try and select 500KHz with no luck. This is happening on different supplies on the same PCB and different PCBs. -- I would suspect a design error but we reviewed the schematic and PCB and have not found anything that could cause this.

I can send the schematic circuit if desired.

Thanks for the help.

BR.

WB