This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5180: Specs

Part Number: LM5180

Hello,

Can someone help me fill in this table please:

MPN MFR Function/Topology Max. Output Current Output-Input Type Output Polarity Output Voltage
LM5180NGUR TI xx xx Adjustable/Fixed Positive 1.8-48V

Please select from the below values for the parameters:-

1) Function/Topology:-

Step Down, Step Up or Step Up/Down

 

2) Output-Input type:-

• Adjustable: Adjustable over a voltage range.

• Adjustable/Fixed: Can be either adjustable over a range of voltages or can supply one or more fixed outputs.

• Fixed: One or more fixed voltages

• Selectable: Outputs that can be set to one of several fixed voltages.

 

3) Output Polarity:-

Positive

Negative

Positive/Negative

I'd appreciate the help!