This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5156: Specs

Part Number: LM5156

Hello,

Can someone help me fill in this table please:

MPN MFR Function/Topology Max. Output Current Output-Input Type Output Polarity Output Voltage
LM5156QDSSRQ1 TI xx 10A in Boost/SEPIC Adjustable xx xx

Please select from the below values for the parameters:-

1) Function/Topology:-

Step Down, Step Up or Step Up/Down

 

2) Output-Input type:-

• Adjustable: Adjustable over a voltage range.

• Adjustable/Fixed: Can be either adjustable over a range of voltages or can supply one or more fixed outputs.

• Fixed: One or more fixed voltages

• Selectable: Outputs that can be set to one of several fixed voltages.

 

3) Output Polarity:-

Positive

Negative

Positive/Negative

I'd appreciate the help!

  • Hi Alexander Walton,

    thank you for using the E2E forum.
    The LM5156 is a wide VIN nonsynchronous controller for Boost, Flyback or SEPIC implementations.
    This means this device can be used for both step-up and step-up/down topologies with a wide input and output voltage range.

    For more details on possible applications and specifications, please refer to the datasheet available on the product page:
    https://www.ti.com/product/LM5156

    If you have further questions, please let me know.

    Best regards,
    Niklas

  • Hi Alexander Walton,

    I hope we were able to answer your question.
    As there are no further comments, I will close this thread for now.
    If you have additional question, feel free to reply below to re-open the thread.

    Best regards,
    Niklas