Other Parts Discussed in Thread: AWR1843
Immediately, I have two questions.
1. Default values of SW_B0 and SW_B1 of LP873347RHDT
When using this IC as a switching regulator, what voltage will come out if no program is written?
By the way, how to connect the circuit is as shown in the attached file.
Please tell me the values of VOUT1 and VOUT2 respectively.
(Input voltage is direct current of 3.3 V)
2. Pin for writing the program
Is it correct to write the LP873347RHDT program (output voltage setting, etc.) on pins 17 and 18?
(As I said in another thread, I heard that there is no problem connecting to the I2C pins (G14, F13) of AWR1843.)