Hi
We would like to know how to calculate the resistance for feedback circuit.
here is the application:
- Vin = 5V
- Vout = 6V for 2 LEDs in serial
- Iout = 350mA
Thanks.
Jack
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
We would like to know how to calculate the resistance for feedback circuit.
here is the application:
Thanks.
Jack
hi Jack
The FB resistor can be set according to the current requirement. Here is the formula: R=250mV/ILED.
So for this case, R=250mV/350mA=0.714ohm.
hi Jack
Basically, LED driver works as a current source. In this case, LED current will be regulated at 350mA and once the current is fixed, the voltage drop on LED will be 6V with 2 LED in series.
Hi Mason,
I have a question to check with you.
From the formula "R=250mV/ILED. ", it seems like the feedback voltage is regulated to 250 mV instead of 200mV. Should we use 250mV or 200mV?

Moreover, please correct me if I am wrong, TPS61165 can be use as a buck LED driver, right. for example, 12Vin to 5Vout to drive one LED.
Thanks.
hi Jack
Sorry the value should be 200mV rather than 250mV. Besides, TPS61165 cannot work as a buck LED driver. It only supports boost topology.