Other Parts Discussed in Thread: TPS62135, TPS62912, TPS65400
I designed in TPS54495PWP on my latest board to create 5V and 3.3V from 12V, as seen below:
As designed, noise on both Vout's was coupling onto other parts of my board.
For 5V out, base current draw is around 7mA. When measured after FB11, there is a 1.3kHz sawtooth waveform with a Vpp of 135mV. I experimented with different output capacitance and ferrite bead values, with the best improvement resulting from removing the ferrite bead, short across the pads, and up the output capacitance to 147uF. The sawtooth frequency increased to 2.8kHz and Vpp of 110mV.
For 3.3V out, base current draw is around 250mA. When measured after FB8, there is a 38kHz sharktooth waveform with a Vpp of 70mV. In this case, by removing and shorting the Ferrite bead and changing total output capaciatnce to 47uF, I was able to improve to ~65kHz waveform at only 20mVpp.
At this point, I would appreciate any guidance you could provide to improve the noise levels on these buses and any changes or improvements that are needed to the overall design. My design is very sensitive to audio frequencies, so minimizing or eliminating them is important.