Other Parts Discussed in Thread: ISO1541, TIDA-01093
Hello,
We are working on a battery design where it is required to monitor between 20 to 23 Li-ion cells in series. Due to availability and experience with BQ76940 this is our IC of choice for the design. As BQ76940 can monitor up to 15S cells, we need to use two ICs in a stacked configuration as shown below. To communicate with both ICs over I2C we plan to use I2C Isolator ISO1541 on the top side IC.
The question that remains is, can we use two different model variants of BQ76940 IC to have unique I2C addressing for both low side and high side IC and if so, can we then remove the FET and MCU control line (as shown in RED on the picture below) to the ISO1541, that is shown in TIDA-01093, as we should be able to uniquely address the BQ76940 ICs?
To have the two ICs with unique I2C addresses we want to select:
- BQ7694002 with I2C address 0x08
- BQ7694006 with I2C address 0x18
Looking forward to your reply and opinion.
Many thanks and kind regards,
Matej