Other Parts Discussed in Thread: LM3404, LM3404FSTDIMEV, LM3402
The below schematic is the same one as in the original post. I understand that the original post will be visible while looking at this related question.
As originally discussed in the previous post we were driving multiple LM3404 drivers with the output of one AM26LS32. The AM26LS 32 was excessively loaded down and could not produce an output signal capable of turning on the LM3404 sufficiently to turn on the LEDs at the lower intensity levels. At higher intensity levels, longer PWM pulse width, the LEDs would turn on. I'm guessing, but I would think it is the input capacitance of the multiple external mosfets that loaded down the AM26LS32.
By using a additional mosfet to drive all the dim pins, that is drive the external mosfets, (on the right side of the schematic above) we were able to keep from loading down the AM26LS32. All the lower intensity levels that did not work previously now worked. All 15 different intensity levels now functioned and we were able to get the 25,000 to 1 contrast ratio.
However, we still have a flickering at the lower intensities. Our PWM base frequency is in the 200 to 250 Hz range. We tried varying the base frequency thinking that multiples of 60 Hz could be the problem. We used a function generator for precise control. But when we thought we had a flicker free frequency, say 230 Hz, the next day the flicker would be back and a different frequency would appear to be flicker free.
Questions:
1. Do you have any idea on how to eliminate the flickering? We have tried more than one power supply.
2. We do not have resistor in series with the gate of the external mosfets. The TI eval board LM3404FSTDIMEV uses a 1 ohm resistor. Do you feel we should add a series resistor to the external mosfet gate and how do you calculate the resistor value?
Thank you for your help.