This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022: TINA Simulation, Boost 12VDC->65VDC@1A

Part Number: LM5022

snvm450.TSC

Hi Teams,

I want to build a boost power supply, converting +12V to +65VDC, max Iout 1A.

Webench recommends the LM5022. So I build the TINA simulation file. Everything is nice, except the output voltage cannot be regulated to 65V. According to the webench report, the FB voltage divider was set as 18.2k:360, and the ouput voltage is 61V.

Cause my target is 65V, so I modified the divider aiming to get a higher output. However, no matter by decreasing RFB1(200) or increasing RFB2(20k). The output was still at 61, and not going higher any further.

On the contrary, getting a lower output can be easily achieved by decreasing RFB2 or increasing RFB1.

Can you kindly help to solve this problem?

The .TSC file is attached.

Thanks and BRs.

Marsh.