This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: when clamped V_COMP to 2.7V

Guru 11170 points
Part Number: UCC28950
Other Parts Discussed in Thread: UCC28951

Hello E2E,

I know that the UCC28950 has issue when overcurrent protection behavior with maximum duty operation from following thread information.
I also learned that clamping the COMP pin to 2.7V is an appropriate countermeasure.

e2e.ti.com/.../ucc28950-at-current-limit-and-maximum-duty-cycle

Please let me know the side effects of this measure.

COMP terminal voltage for hiccup operation and transition to latch stop mode
Are you using it?
Is the COMP terminal voltage used for functions other than the above?
What does the UCC28950 do when overcurrent occurs at maximum Duty when the COMP terminal voltage is clamped to 2.7V?

Best regards,
ACGUY