Other Parts Discussed in Thread: TPS7A25
Hi Team,
There is a good news that we have a chance to replace "CAT6201 "
Do we have a solution to replace "CAT6201 " ?
The URL below is "CAT6201" datasheet
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kygo,
The best options to replace CAT6201 would be TPS7A25. LP2986 has a lower Iout, but could work if the current requirements are not needed.
| LP2986 | TPS7A25 | |
| AEC Q100 | NO | NO |
| Output Options | Adjustable Output, Fixed Output | Adjustable Output, Fixed Output |
| Iout (Max) (A) | 0.2 | 0.3 |
| Vin (Max) (V) | 16 | 18 |
| Vin (Min) (V) | 2.1 | 2.4 |
| Vout (Max) (V) | 5 | 17.64 |
| Vout (Min) (V) | 1.23 | 1.24 |
| Fixed Output Options (V) | 3, 3.3, 5 | 1.25, 1.8, 2.5, 3.3, 5 |
| Enable | YES | YES |
| Power Good | YES | YES |
| Output Capacitor Type | Non-Ceramic | Ceramic |
| PSRR @ 100KHz (dB) | 42 | 22 |
| Noise (uVrms) | 160 | 300 |
| Accuracy (%) | 3 | 1 |
| Vdo (Typ) (mV) | 180 | 210 |
| Iq (Typ) (mA) | 0.1 | 0.002 |
| Thermal Resistance θJA (°C/W) | 38 | 73.3 |
| Min Package Area (mm2) | 14.7 | 4 |
| Package Type | SOIC, VSSOP, WSON |
WSON |
Thanks,
Prakash L