hi team :
recently i found a issue when i use the TPS7A7001 device. And there may be some leakage from the load, and cause the Vout to -0.2V ,then the TPS7A7001 will not output anymore. But i add 300Ω between Vout and GND, then the issue is fixed. would you share any comments about this protection logic? And if there any recommend resistors value?