This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS561201: Alternate part request for TPS561201

Part Number: TPS561201


Hi All,

We considered TPS561201 part in our design.

We would like to check on similar pin mapping switching regulator availability which accepts 2.7V input range?

Current rating from 500mA to 1A is acceptable.

 Please suggest any pin to pin equivalent for TPS561201 which accepts input voltage range from 2.7V.

Regards,

Harish.