Other Parts Discussed in Thread: TPS53355, TPS548B28, LM27402
Hi,
I am looking for a Buck Regulator with below requirement also which can support transient of 25A to 30A
Vin=3.3V, Vout= 0.8V, Iout=20A to 25A
Can you please suggest a regulator which can handle higher transients.
Minimum Vin requirement is 3V. What is maximum transient that TPS548B27 can handle.