Other Parts Discussed in Thread: BQ79616-Q1, BQ769142
Hi,
I am trying to implement the sample code given in "BQ79616-Q1 Software Design Reference" document. I have connected an MCU <->BQ79616EVM through the J17 connector. I have connected J17.5 to MCU_GND, J17.6 to MCU_3v3, J17.7 to MCU_UARTTX and J17.8 to MCU_UARTRX pins. I have then send the WAKE Ping and I saw the D1 light up. Following the document, I have sent the following messages:
{D0, 03, 4C, 00, FC, 24}, {D0, 03, 09, 01, 0F, 74}, {D0, 03, 06, 00, CB, 44}, {D0, 03, 08, 02, 4E, E5}, {90, 00, 03, 08, 01, D2, 1D}, {C0, 03, 4C, 00, F8, E4}
After the broadcast read command I expected for the EVM to send a message back but there is no response from the EVM. I am sending you scoped TX and RX pins of EVM attached.
Can you please help me with this issue? What am I doing wrong?
Regards,
Figure 1: Overall communication (MCU_TX-> Blue, MCU_RX -> Red)

Figure 2: Zoomed in to message (MCU_TX-> Blue, MCU_RX -> Red)