This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51200: VO oscillating

Other Parts Discussed in Thread: TPS51200

Hello,

I'm seeing significant oscillation on the output of a TPS51200 which seems to be part of the reasons why my board is having calibration issues (i.e. DDR2 initialization/calibration fails). The measurements show a 5 MHz oscillation (sine wave) with more than 600 mV peak-to-peak (see scope screenshot).

DC coupling:

AC coupling:

On top of that, the device gets extremely hot, even with the DDR2 memory (MT47H32M16HR-25E) inactive.

Now, I'm wondering whether this is a clear indication that the regulator is broken or whether there's another reason why it doesn't operate correctly. I've been using it on a prototype. Initially the supply voltage (VIN) had a significant ripple (about +/- 150mV; ~300 kHz; spikes) coming from DC-to-DC converters. This has been fixed by replacing them with the output of a linear (lab) power supply but it might have already caused some damage to the regulator.

This issue is consistent throughout all 3 prototypes (same revision) that I had built.

I've also checked whether this is an issue only under load. However, removing the ferrite bead (FB23) didn't make a difference (see schematic & scope screenshots). In fact, the device still gets extremely hot.

AC coupling:

Also, I checked all other inputs (REFIN 0.9V, VLDOIN 1.8V, VIN 2.5V)  and outputs (PGOOD -> ~0V indicating the failure; REFOUT 0.9V) which measure correctly and do not show any oscillation.

I really need to make sure that I'm in fact looking at 3 broken regulator as a rework is quite involved. Also, I'm wondering how sensitive these parts are with respect to supply voltage ripples.

I appreciate your help!

Regards,

Steffen

  • Hi Steffen,

    I don't think that the chip is broken. Maybe this will help:

    - C104/105 have to be close to pin 3 (remove FB23 completely).

    - Check the capacitors C104, C105 - are they broken? Try 10uF.

    - C103 has to be close to pin 2.

    - C94 close to pin 1.

    - Place 1k or more on pin 5 (between C105 and pin 5). Disconnect pin 5 from pin 3.

    - Do you supply anything with the pin 6? Or it is just a test-point?

    - Put 1k or more on pin7.

  • Hello Paul,

    thanks for your quick response.

    As you can see from the layout image below, most of the things you recommended to check can be confirmed:

    • C104/105 are relatively close to pin 3
    • C103 is close to pin 2
    • C94 is close to pin 1

    I forgot to mention that I already removed FB23 completely and shorted its pads - the same oscillation (although with a lower amplitude and slightly different frequency) remained. As far as the connection between pins 3 & 5 goes: This essentially follows the design example 1 in the datasheet (DDR2 on 3.3 VIN) although I'm using 2.5V VIN here. I understand that you're suggesting to squeeze in a 1kOhm resistor between C105 & pin 5 which will be rather complicated to hack but I'll try (once I confirmed that the capacitors C104 & C105 are OK and replaced with 10uF as you suggested). Can you tell me the motivation for this experiment?

    As far as the output of pin 6 goes: It supplies the DDR2 memory's VREF input.

    Also, can you explain why you'd put a 1kOhm resistor on pin 7 (EN)?

    Just to give some more background information: The design I used is based on a reference design from a development board (which works). Here is the schematic and layout portion for comparison purposed:

     

    I appreciate your help!

    Regards,

    Steffen

  • Paul,

    I guess the reason why you're suggesting to squeeze in a 1kOhm resistor between C105 & pin 5 is to improve loop-stability according to the recommendations in the datasheet with respect to the output capacitor (in case they don't have a sufficiently low ESR). Let me know if this is your motivation for trying this out.

    Thanks,

    Steffen

  • Hi Paul,

    just as an update, the output capacitors on both, the reference design (C182 & C200) as well as my own design (C104 & C105) are the exact same ones (same manufacturer, same manufacturer P/N). That is, ESR and ESL characteristics (which seem to be somehow critical as far as the datasheet goes) are the same. Again, the reference design works just fine.

    Regards,

    Steffen

  • Paul,

    it seems like it was indeed a problem with the output capacitors (C104 & C105). Unfortunately I didn't have any with 10uF, neither 22uF like the ones installed on the board. So I used two 33uF ones to replace the broken ones and all the oscillations went away. Also, the device's operating temperature went down significantly (it just gets warm a tiny bit as opposed to hot like before).

    Thanks for your recommendations. This saved me a lot of time (and money).

    -Steffen

     

  • :-)

    Glad to help.

    Paul