This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5045: Supply 200V to the H-bridge

Part Number: LM5045


Hi Team,

Our customer would like to use the LM5045 in this configuration.

I want to supply the power to the H-bridge from a 200V input voltage. I will use a buck converter externally to make the Vcc voltage (12V). After that I will connect BST1 and BST2 to the same Vcc voltage and HS1 and HS2 to the GND. Then when I use a gate transformer for the switching outputs to turn-on/off the Mosfet's to switch 200V, will the controller function as normal?

Regards,

Danilo