This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25944A: Reverse current protection

Part Number: TPS25944A

Hi Team,

Our customer would like to clarify about the reverse current protection of the TPS25944A. According to our customer,

We have designed it into our system and we are having some issues and the datasheet isn't very clear on some points. It's about the Reverse Current Protection behavior.

In the case when you have two power system Or'd together and one is 10mV greater than the other one, the device with the lower voltage is supposed to shut down.

It seems like PGOOD should go low, correct?

There are several different failure modes, and the behaviors of FLT, PGOOD, VOUT, and EN are all important to us.

Regards,

Danilo