This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5176: LM5176 12V TO 5V Schematic review / check

Part Number: LM5176

Hello,

Can you please help to review my schematic of LM5176? That is for 12V TO 5V solution. Thanks.

25-LM5176 .pdf

  • Hi Hins,

    thank you for using the E2E forum.

    I have a few comments / questions regarding your schematic.

    What is input supply voltage range ?

    Your total capacity of the input caps look low - may you check if this would fit for your input ripple 
    (you can also use the design calculator for checking that: LM5176 data sheet, product information and support | TI.com

    The voltage divider on mode might be wrong - no sure about the intention but for setting the mode only a pull down resistor is required as there in an internal current source.
    Please see also datasheet for more details

    Why do you use two transistors in parallel - this might not be required based on the design information I have seen in the schematic

    Best regards,

     Stefan

  • Hi Stefan,

    Please review the clarification  information. There are two parts for the LM5176 application.

    1. For LM5176 6-38V BUCK-BOOST 12V, the input supply voltage range is 6V to 38V, it is Automotive battery power, want to use LM5176 to Buck-Boost output 12V.  i.e. When the automotive battery is 6V, it needs to boost output 12V. When the automotive battery is 38V, it needs to buck output 12V.

    2. For LM5176 VCC_SRC_FET 12V BUCK 5V, the input supply voltage range is 12V, want to use LM5176 to buck output 5V.

    In the schematic, R542 and R582 don't need to install it. If confirm the mode only a pull down resistor is required, I will delete it later.

    For two transistors in parallel, that is refer to LM5176EVM-HP Schematic. Thanks.

    24-25-LM5176.pdf

  • Hi Hins,

    thanks for the details, will review and come back in the next 2-3 days.

    Best regards, 

     Stefan

  • Hi Hins,

    just a few minor items:

    for the first schematic:

    C slope looks a little bit low (470pF would be better)

    MODE only requires a resistor to GND

    for the second schematic:

    C slope looks a little bit low (470pF would be better)

    MODE only requires a resistor to GND

    Note: do you also know the Design Calculator tool - this can help a lot for getting this info as well:

    LM5176 data sheet, product information and support | TI.com

    Best regards,

    Stefan

  • Hi Hins,

    I have not seen an update on this thread for the last 24 days.
    So I assume the issue is solved.
    In this case it would be great to press the is solved button.

    If there is still something open, just let me know with the new details.

    Best regards,
     Stefan