Hi,
Customer Kohler asks:
Recall several months ago TI helped Kohler understand why a TPS61090 was having oscillation problems. It was due to too low ESR on the bulk capacitance. Recently Kohler updated the schematic to the following (C20 was previously 100µF, however due to design change now need more energy stored at 5.5V in case power is lost):
New C20: UVR1A222MPD
Previous C20: TPSD107M016R0150
C3: EMK107BJ225KA-T

Kohler is trying to ensure this design meets the datasheet’s ESR requirement.
The concern is that the EMK107BJ225KA-T and UVR1A222MPD in parallel may result in an ESR below 30mOhms.
Additional concern is in this design, the bulk capacitor C20 cannot be located nearby the TPS61090 due to physical space constraints. The image below shows the bulk capacitor planned location. You can see the location of U1 is between the yellow tantalums present on the previous prototype board.

Can you help Kohler understand if the design will be stable and how to best determine or evaluate?
Thanks,
HSG