This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92511: Part will not simulate in PSpice, missing sub circuit definition

Part Number: TPS92511


Evaluating the TPS92511 LED driver for incorporation into a new product.  This device will not simulate within Pspice.  I sent the .lib file to Cadence to see if they had the same problem with it, and their tech said that it is missing a sub-circuit definition, so the part will not simulate. The .lib file and olb file were downloaded from the TI product information page.  The sample project on the web page also does not run for the same reason.

It errors on not finding a ".SUBCKT SWhyste". So it's missing a sub-circuit definition that's probably called from another .SUBCKT,  is what Cadence told me.

The Output Window reads:  ERROR(ORPSIM-15108): Subcircuit SWhyste used by X_U32X_U10_U1X_S1 is undefined

Is there another place to download a good .lib file for this part, or maybe one that is not encrypted?