Hello, I'm hoping to get some advice on a small package LED Driver which can provide drive to 1-4 LEDs. The LEDs are small 3020 package with 3.3V 100ma power requirement. The input voltage will be from a USB connection so 2.7-5.5V with 750mA. I also need the ability to dim the LEDs with a DC control voltage not with PWM.