This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

40 W, Low-Parts-Count, Multi-Output, Galvanically Isolated DC/DC?

Other Parts Discussed in Thread: UCC2803

How to make a lowest-parts-count, small-footprint, 40 W, galvanically isolated, DC/DC converter?

Input: 12 V to 24 V

Output: 4 V to 9 V @ 10 W x 4

the outputs should be isolated from each other.

I'm assuming a device or topology that outputs 40 watts of non-isolated, unrectified power, and then a separate transformer+rectifier for each output.