Other Parts Discussed in Thread: TPS543C20, , TPS543B20
Hi,
In my board I have 2x syncs TPS543C20RVFR, can I replace it with TPS543C20ARVFR without problems?
Or I need to do a few tests before?
From the datasheet I saw that the only changes are the input voltage (4V-14V to 4V-16V) and (Integrated 3/0.9-mΩ Stacked NexFET Power) to (Integrated 3.4/0.9-mΩ Stacked NexFET
Power)
I'm using 12V input.