This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24298: ISYS limit

Part Number: BQ24298


Hi,

I see in 7.3 of the BQ24298 datasheet, it says the recommended maximum for SYS output current is 3.5 A.

I am wondering if it is safe to temporarily push above 3.5 A when operating with battery and without DC source. In this case, all I see being an issue is the current limit of BATFAT (Q4), which I can't find listed in the datasheet.

Thanks,

Luca