Dear experts,
When using LM25117PMHE/NOPB, It is found that the VCC pin of the power chip has a spike that is frequently consistently with the driving frequency of the MOSFet (≈221kHz). The value of spike is about 25V. And the duration is about 12ns. The peak appears at the same time when the upper tube is turned on. The waveform and circuit are shown in the attachment;
Since the diode D47 is connected in series between the VCC pin and the capacitor, it cannot be removed, and it cannot be replaced with a 0Ω resistor due to the special package. Based on the current circuit, is there any suitable BOM rectification measures to adjust the peak? Or does the spike have any effect on the application and life of the chip, thank you!