This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54531: TPS54531 Startup Issues

Part Number: TPS54531


Hello,

We are having sporadic startup issues with a design that implements a TPS54531, this design takes 5V to 3.3V with an average load of ~2A.

Cin = 9.4uF (x2 4.7uF in parallel) ; Css = 8.2nF ; Rcomp = 51.1k ; Ccomp = 820pF ; Ccomp2 = 15pF ; L = 3.3uH ; Cout = 200uF

The startup wave form will ramp as expected up to 3.3V then after a short period of time (~1ms) the output of the regulator becomes unstable and starts oscillating between ~2V and ~3V every 500ms or so.

If I change the L to 2.2uH from 3.3uH then everything functions as expected, all else remain the same.  Using web bench set to balanced I get the following bode results:

Low F gain       Cross F         Phase Marg.      Gain Marg    Inductor Val

29.83 dB           24.02 kHz     47.09 deg           -17.11 dB     3.3 uH

29.98 dB          26.82 kHz      54.99 deg           -17.39 dB     2.2uH

Is there something we are violating by using the 3.3uH inductor?  We are seeing the failure in roughly 5% of the boards that come off the line.

Thanks,

Brian