Other Parts Discussed in Thread: BQSTUDIO
We made a new design with bq27546 because bq27421 (our preferred option) is out of stock, and you had > 1M bq27546 in stock. Now we see that bq27546 itself is out of stock! Anyway we are using it in our current production run and we have the following programming questions:
1) We will program the required registers (Design Capacity, Terminate Voltage...) at first initialization with our firmware. But since we don't need great precision on the SOC, for simplicity we'd rather use the default Chemistry 0100 (our cell is a regular 1200mAh, 3.7V, 4.2V charging Li-Ion, similar to 18650). Is the bq27546-G1 delivered with this default Chemistry already programmed and ready to use?
2 The only registers values that are not clear to us are the CC Gain and CC Delta (104,0 and 104,4). We use a 20mOhm sense resistor. We don't have an EVM to connect bqStudio to our own PCB. How can we calculate approximate CC values without bqStudio connection? BTW bqStudio reports at start that bq27546 is not supported?
3) In the bq27546 Technical Reference Manual (Literature Number: SLUUB74, May 2015) section 5.11.3.4 (Pack Configuration D) there seems to be an error in the description of bits :
Thanks for your support