This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1HC100-Q1: Pin Connection

Part Number: TPS1HC100-Q1

Hello team,

I received three questions from the customer.

1. The recommended RPROT (protection resistor) is 5kΩ.

Which is more suitable, 4.7kΩ or 5.1kΩ?

2. They would like to fix DIAG_EN, LATCH, and SNS without control.

DIAG_EN (fixed to High): Is it OK to connect the operating voltage 3.3V directly?

LATCH: Is it OK to use RPROT to connect to GND for setting auto entries?

SNS: Since the AD value is not monitored, is it OK to connect to GND with 1kΩ?

3. They would like to set the Current Limit to about 1A (0.7 to 1.3A).

Is 47kΩ the suitable value for RILIM? *They said it is difficult to read from the graph.

Regards,

Masa