This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2561: IEC62368-3

Part Number: TPS2561


I design set-top box have USB port

TPS2561 is designed for USB, and for IEC62386-1 certification.(US-37138-UL)

But TPS2561 doesn't have Input Over Voltage LockOut(or Clamping).

How certificate IEC62386-1 with TPS2561?

Is TPS2561 no longer available for new design?

 

Here's the TI document I saw about Over Voltage LockOut(or Clamping) - slvafb0

More recently IEC62368-3 Safety aspects for DC power transfer through communication cables and ports has
emerged. This standard mandates that under single fault conditions in the PSE with a fixed, single output
voltage, the output of the PSE shall not exceed 130% of the nominal rated output voltage.

In practice, this means that if an upstream voltage regulator fails and applies a higher voltage to the USB power
switch, the output must not exceed 6.5 V. Most traditional USB power switches are rated for 5 V with an absolute
maximum voltage rating in the range of 6 V. If the upstream failure applies 12 V to the USB switch it is likely to
fail and it cannot be guaranteed that it will not fail in short thus applying the 12 V to output port.

  • Hi, 

    It's on-going for the IEC62368 cert. 

    Correct. It doesn't include the OVP protection of input. And also can't exceed the ABS of VOUT. 

    Don't have the roadmap for the function.

    If you have any other concern, contact me any time.

    If you think resolved, please help click 'Issue is solved button'.

    Thanks.