Other Parts Discussed in Thread: CSD17318Q2
Team,
Can you please help with the below?
I have a question about the CSD17313Q2 mosfet (see Datasheet SLPS260E page 3).
According to the information on VGS(th), 3.0V is sufficient.
But in the features it says that the part is "5V drive optimized".
Questions:
-What does "5V drive optimized" means exactly? What would be the difference if driven at 3.0-3.3V?
-Can this Mosfet be driven with 3.0- 3.3V level without any problems ?
- If not, is there an alternative in the same housing that can do this ?
Thanks in advance,
A