This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54232: Schematic & Layout review

Part Number: TPS54232

Hi Team,

There is a good new that we DIN TPS54232D 5V to 3V3 DCDC

And there have one thing need your support!
Please help check this SCH & layout, THX (please refer to attachment )

2437.Layout.pptx

  • Hi Kygo

    Glad to hear the DWIN news! Here are my comments:

    1. Regarding the boot cap For the boot cap, I would suggest to use 220nF or even 470nF to avoid BOOT UVLO risk. If customer does not want to change the boot cap value, I would suggest to reduce the inductor value to 2.2uH. 

    2.For the layout, I would recommend to remove the GND copper which covers around the pins especially the BOOT and PH pin since they are noisy. 

    BR

    Ruby