Hi team,
Could you please help to check our datasheet for correction. Here it is.
I am fairly sure there is an error in the datasheet for LM3410 ICs.
Only found out once I got the board and started hooking thinkings up.
Application examples page.
8.2.6, OVP protection
R3 is basically in series with the pin 3, feedback pin and the R1 resistor that determines current through the LED. In the LM3410, The feedback voltage is 200mV, meaning the values for R1(4 Ohm) is right to deliver 50mA. However R1 value is 100 ohms and will reduce the current to 200mV/(100+4) = 1.9mA
The R3 seems to be a current limiter resistor for the Zener diode. So a proper schematic seems to be one where it's in series with the Zener. So the feedback pin will go direct to R1, not go through R3 first.
Figure 14 too.
So I think the intentions are correct, because in 8.1.1.7 it says Zener diode D2 and resistor R3 is placed from V OUT in parallel with the string of LEDs.
Thank you so much.
Best regards,