Hi E2E,
I made a design using the webench design tool for a flyback switching power supply that receives 40-300(AC) as input and gives 5 different outputs
with these parameters below
1) 24 V - 0.5 A
2) 10 V - 0.7 A
3) -10 V - 0.7 A
4) 5 V - 0.7 A
5) 3.3 V - 1 A
6)15 V (auxiliary)
Switching frequency = 100 Khz
. I am pretty happy with the design and even made a few changes to better fit my application, but I don't know how to interpret the transformer values it gives me because webbench give me the value for only one output. I haven't really studied these types of transformers and I'm not sure how to communicate this information to a supplier to get prototype part for testing. Any advice, or too can design this transformer?
here is my circuit from tina ti
I'm looking forward for your answer