This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ULN2003AI: VOH for ULN2003AINSR and ULN2003ANSR

Part Number: ULN2003AI
Other Parts Discussed in Thread: ULN2003A

Hello Team, 

Customer considers to use ULN2003AINSR as alternative for ULN2003ANSR to avoid delivery issue.

According to the datasheet, we found the differences are VOH and temperature range.

However, they cannot accept VOH MIN -50mV.

Can ULN2003AI meet VOH MIN -20mV under less than 70C environment? They do not use this device at temperatures above 70C. Please give your advice. Thank you!

 

Temperature range

ULN2003A:-40 to 70C

ULN2003AI:-40 to 105C

 

VOH

ULN2003A:MIN -20mV

ULN2003AI:MIN -50mV

Best regards,