This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62811-Q1: Efficiency, line regulation & Load regulation data @ temperature -40C,105C

Part Number: TPS62811-Q1

Hi there, 

can you please help me with the following data as it's not in the data sheet:

TPS6281120QWRWYRQ1 

@ -40C 

Iload(Open load) :  2.75V = , 3.3V = , 6V =

 Iload(100mA) :  2.75V =  , 3.3V = , 6V =

 Iload(300mA) :  2.75V =  , 3.3V = , 6V =  

 Iload(650mA) :  2.75V =  , 3.3V = , 6V =

 

@ 105C

 Iload(Open load) :  2.75V = , 3.3V = , 6V =

 Iload(100mA) :  2.75V =  , 3.3V = , 6V =

 Iload(300mA) :  2.75V =  , 3.3V = , 6V =  

 Iload(650mA) :  2.75V =  , 3.3V = , 6V =

 

Thanks,

Oguz