Part Number: LM5116
Hello,
I am in a situation where i'd like to check that the LM5116 will not be damaged due to an input condition. The situation is as follows:
Upstream of the LM5116 there is a unidirectional TVS from VIN to GND. If there is a negative transient, then the voltage from Vin to GND is clamped to about -0.7V. This breaks the datasheet specification of -0.3V.
If a diode is added from the power positive line to the Vin pin, will this protect against the reverse current situation from the negative transient described above?
Aidan