This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2679: LM2679T-12/NOPB design review please

Part Number: LM2679


Using LM2679T-12/NOPB, a circuit that outputs 24V input to 12V/5A was constructed. 
Measuring the output terminal measures 12V.
However, when a load of 12V/1A is applied, only about 3V to 4V is output.
What's wrong with my circuit?