This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65916: Powering On TPS659163RGZT

Part Number: TPS65916
Other Parts Discussed in Thread: AM5706

Hi, I( am planning to use  TPS659163RGZT to power AM5706 processor in my board. I am planning to use it with out power on switch. That means Once i give external power the board should start working. Can I pull down the PWRON signal so it will be having as a switch on event,(which is there all the time). Or can I utilise POWERHOLD pin to achieve this. What is the main functionality of POWERHOLD signal, it was not clear in datasheet. Is there in OTP memory required to do this.

Is there any reference design available with this setup. Please help me to sort out this issue.