Hi I have a problem regarding the simulation of TPS629210E. I have connected the IC in PSPICE for TI according the schematic from page 89 of your datasheet ( TPS629210E 1-A, 3-V to 17-V, –55°C to +150°C Low IQ Buck Converter datasheet (ti.com) ), and on the output I got exponential curve 892 nV to 929 nV for simulation interval 0-3ms.
Component values are : L1=4.7uH, C2=22uF, RT=100ohm, R2=11.5k, R1=52.3k.
Transient simulation settings : Maximum step size : 100ns
Could you please advise me in terms of simulation parameters which I have to apply in order to have successful transient response?