Is there an isolated gate driver than can accept 12V to 24V in?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there an isolated gate driver than can accept 12V to 24V in?
Hi, Johny,
Yes, UCC23513 and the related devices can accept a 12-24V input signal with the proper resistor to limit the current to between 7 and 14 mA.
Please see section 9.2.2.1 Selecting the Input Resistor of the datasheet for further information.
We have an excel tool that helps you select the correct resister value. You can find it here.
If this resolved your question, please press the Green button, otherwise, let me know what further questions you have.
Best regards,
Don