Other Parts Discussed in Thread: LM317
Hello,
I found TPS7B6950QDCYRQ showed two different lead frames on X-ray vision. Is this normal that lead frame can vary? Otherwise, Has been any PCN released ?
- DC21

- DC21

Best regards
Yeon Kwang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I found TPS7B6950QDCYRQ showed two different lead frames on X-ray vision. Is this normal that lead frame can vary? Otherwise, Has been any PCN released ?


Best regards
Yeon Kwang
Hi Yeon,
Yes this is normal because the assembly site is a subcontractor and so they can use different lead frames. I recently supported a very similar question for the LM317 in the DCY package which had the same result. See the attached PPT that shows a comparison of the observed lead frame and the lead frame drawing from the subcontractor.
Customer question LM317DCY.pptx
Regards,
Nick
Hi Nick,
Thanks for the kind answer. They have the same country of origin except for DC as below. Is this normal even in same assembly site ?
1. DC : 2130, CS0:DM5, CC0:USA , AS0:NFM, AC0: CHN
2. DC : 2133, CS0:DM5, CC0:USA , AS0:NFM, AC0: CHN
Best regards,
Yeon
Hi Yeon,
Do you have a lot trace code you can share? I will look further into this if you can provide this.
Thanks,
Nick