This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5118: Noise on FB pin from FET Gate.

Part Number: LM5118

But the noise I am seeing on the FB pin cause the output to fluctuate in a random manner.

I have removed the Control OPAMP from the design which makes the output a max of 24V @ 2A from a 45V input.

The noise is the same with or without the external drive.

I would like to clean this up.  

The adjustment ranges is 24V down to 16V. But that is for latter.

Having trouble uploading images.  Will add more...