Part Number: BQ27531-G1
Hello,
I am using BQ27531-G1 gas gauge. During the learn cycle, gauge learned cycle count=2 (Data Memory > Gas Gauging > State > Cycle Count 0 =2) in Bq studio. But before generating a golden image, I have changed the Cycle count 0 = 0 and then generated a golden image.
As per the BQ27531-G1 TRM , one cycle occurs when accumulated discharge ≥ CC Threshold. In our CC Threshold=4000mAh (which is normally set to 90% of the design capacity ,4400mAh). When the gauge accumulates enough discharge capacity equal to CC Threshold, it increments CycleCount() by 1.I have performed complete discarging and charging of battery but still the cycle count is 0. Why it is not changing?
Regards,
Janhavi Rane