Hi,
I have used the TPS2373-EVM758 for 5V POE output but now I need to change it to 12V. Can you share an altium project with the TPS2373-3RGW and UCC2897ARGPR which outputs 12V? both 50W and 70W is good for the project. I spent too much time on designing 5V output but unfortunately changing it to 12V is not that simple as far as I understood from the topics in the forum.
I will be really glad and save too much time if you send me the altium design files.
With kind regards,
Ahmet