Other Parts Discussed in Thread: TPS65262, TPS65811
Hi Team,
There is a good new that we could DIN TI product!
Do we have a solution that could me following spec? THX
PMIC Spec. |
||
1 |
Vin |
4V~30V(Maximum input voltage minimum acceptable17V) |
2 |
Vout(3 ~4channel(LVBUCK)+LDO) |
VO1:3.3V(300mA) |
VO2:1.8V(600mA) |
||
VO3:1.2V(>=1A) |
||
LVO:2.9V(300mA) |
||
3 |
Fixed Switching Freq. |
2.1MHz |
4 |
Power good function |
Need |
5 |
Over Current protection |
Need |
6 |
Output voltages Power Sequence can be adjusted |
Need |
7 |
Working temp. |
-40~125℃ |
8 |
Package |
≦4x4mm |