Part Number: LM3671MF-1.8EV
We are actually using the LM3671MF-3.3 device but it doesn't appear in the selection when creating this thread. Upon application of 5V power (yellow trace), the 3.3V output of the LM3671 has a "stepped" startup that is causing our processor to improperly power on reset at times. The load is relatively low mA but the output ripple is minimal so I believe it is running properly, it just starts up very janky.